Loading
Blog | Life Sciences
Recent ActivityRecent Activity

Set Up a Single Use System for Success: Part 2

Create a solid foundation for your life sciences facility by focusing on key areas before you build.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Two life sciences professionals wearing coveralls, masks and safety glasses interact with pharmaceutical production equipment inside a brightly lit facility.

In Part 1 of this blog, we made the case for small and mid-size biological producers to adopt a modern distributed control system (DCS) as they incorporate single-use systems in their facilities. It’s an approach that makes an impact both in the present and the future by creating a more flexible operation that can scale up or down with ease. We already explored how the right DCS choice affects two areas:

  • Network infrastructure by simplifying connections and providing seamless data access
  • Operational flexibility by reducing the effort involved in tech transfer and process development

We’ll finish exploring the benefits by covering four additional areas that can help you meet regulatory requirements, reduce validation effort, incorporate newer digital technologies and analytics, and lower your total cost of ownership.

Technology standardization

The more that customized technology and functionality is designed into a single-use facility, the more that specialized knowledge is required for design, operation, and maintenance activities. This requirement for specialized knowledge should prompt producers to establish and leverage standards as much as possible.

Standards such as the International Society of Automation’s (ISA) ISA-88 (1), ISA-18.2 (2), and ISA-101 (3) help create a consistent design approach across multiple pieces of equipment for functions, including procedural control, alarm management, and human-machine interface (HMI) style. These standards can be easily enabled when configuring modern control systems using commercial off-the-shelf software libraries. By using these class-based libraries, equipment vendors can create application-specific software with less time and development cost.

These libraries also smooth the way for those who inherit equipment — such as validation teams, process engineers, and support technicians — because the software is lower risk, provides consistent information, and is easy to maintain.

The libraries also include standard data structures for specific classes of devices, such as pumps, valves, and others. These data structures provide the basis of constructing analytics for equipment, helping producers increase process performance or equipment uptime in the long run.

Operator experience

The user experience of operations staff is too often left out of automation projects. But producers should consider prioritizing the user experience of the control system if they want to create a more efficient workforce. Libraries of reusable class-based objects can be used to create a common user interface style for staff, for instance. For example, a valve will look and feel the same on a tangential flow filtration skid as it does a bioreactor.

Producers should also ensure their visualization system leverages industry standards, such as ISA 101 (3). The standard can help draw operators’ attention to adverse process conditions to help make sure these conditions are seen and dealt with quickly.

Disruptive technologies

New technologies are changing how people work in a single-use facility — perhaps none more so than augmented reality (AR). How can producers apply technology such as AR in a meaningful way in facilities? The best way to find out is for automation engineers to meet with process engineering and operations teams to discuss needs and potential risks that the technology can address.

For example, single-use consumables can require operators to make hundreds of sanitary and aseptic connections during setup. One wrong connection can lead to a costly batch loss. By performing this work in an AR environment, an operator can confirm each connection and reduce the potential for mistakes.

In another scenario, production operators may not have a view of an HMI when they are performing activities such as pumping media, which can result in missing critical alarm notifications. It may be beneficial for operators to wear an AR headset while doing this work so they are more likely to see alarms as they happen.

Cybersecurity

Mitigating cybersecurity risks is a priority for most biologics producers today. A robust cybersecurity approach can help producers protect their sensitive regulatory and process data, while realizing the many benefits of digitalized operations.

Part of this approach involves designing a control system with standards like ISA/International Electrotechnical Commission (IEC) 62443 (4), which is a consensus-based cybersecurity standard for automation. The standard establishes that multiple layers of protection will provide the most redundancy in case a specific security layer fails. This concept is referred to as a defense-in-depth strategy and spans personnel knowledge and awareness, physical security, application, and device security. Some control systems are now certified to this standard.

Common Industrial Protocol (CIP) security-enabled control devices offer another layer of protection. CIP Security is an extension to the CIP from the automation industry association, ODVA. It uses data authenticity, integrity, and confidentiality to protect against attacks on industrial communications. Industrial asset-management software can also provide recovery and automatic back-up capabilities that are critical following a security incident.

Easing the journey to production

A modern, scalable and flexible control system offers a pragmatic approach to developing an automated single-use facility. With the right design choices, this architecture can help producers create a connected, information-driven facility that scales and evolves with their business.

PART 1: FLEXIBILITY AND INFRASTRUCTURE

Published February 9, 2022

Loading
Topics: Life Sciences

John Hatzis
John Hatzis
Global Life Sciences Industry Consultant, Rockwell Automation
John has been with Rockwell Automation for eight years where he has gained expertise using Rockwell solutions in a variety of Life Sciences applications. In his role he also works with BiofabUSA and Biophorum. John has a degree in Chemical Engineering from Worcester Polytechnic Institute.
 
Pete Genest
Pete Genest
Former Strategic Technology Partnerships Leader, Cytiva
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  • Contact Sales
  • Contact Customer Care
  • Contact Technical Support
  • Phone Support
  • General Questions
  1. Chevron LeftChevron Left United States Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right